Eaton Filtration Gas Liquid Separators, Steam Separator

Gas Liquid Separation

Eaton Gas Liquid Separators remove up to 99% of all damage causing moisture and solid particles larger than 10 microns.

Typically installed following an intercooler or aftercooler, the separators are used to remove entrained moisture that would otherwise cause damage in successive stages of compression or to subsequent processes. They're ideal for entrainment removal in primary air lines leading to air-using equipment such as air chucks, air nozzles, and paint spray equipment.

Separators are often installed ahead of steam turbines to protect the turbine blades from the erosive action of wet steam, pipe scale, and other damage-causing entrained solids. They're also installed in steam distribution lines to assure clean, dry steam enters heat exchangers, pressure reducing valves, temperature regulators, meters, and other process equipment.